5/6/2022 12:57 PM | |
Joined: 9/1/2021 Last visit: 5/1/2025 Posts: 6 Rating:
|
The intention is to write a Segmented circular log on a USB, but I don't think this is very reliable because when the USB is plugged in / out, the OpenLogs must be properly activated for correct operation otherwise no file will be created. The idea is therefore to first write to the SD card and then copy a button to the USB, but I don't see the Segmented circular log in the ArchiveLogFile command, what could be the reason for this? What would be an alternative to copy the Segmented circular log to the USB? Thank You, Luc ------------------------------------------------------------------------------------------ |
Last edited by: LPoels at: 05/06/2022 12:59:40Last edited by: Jen_Moderator at: 05/06/2022 13:01:01New subject after splitting Last edited by: LPoels at: 05/06/2022 13:59:30Last edited by: LPoels at: 05/06/2022 14:00:07 |
|
Follow us on