5/18/2022 6:48 PM | |
Posts: 257 Rating:
|
With the introduction of WinCC Unified V16, three different PC Runtime visualisations can be configured in the TIA Portal.
Their licensing depends on the version and power tag. While there is downward compatibility for the respective PC Runtime software licence version and the Power Tags of the respective PC Runtime licence can be increased with a Powerpack, a PC Runtime licence can only be used for your own PC Runtime software. For example, it is not possible to use a SIMATIC WinCC Professional RT licence for a SIMATIC WinCC Advanced RT or SIMATIC WinCC Unified RT and vice versa. Furthermore, unlike WinCC Engineering licences, the individual PC Runtime variants (Advanced, Unified, Professional) cannot be upgraded via Powerpacks, e.g. a SIMATIC WinCC Advanced RT licence to the SIMATIC WinCC Unified RT or SIMATIC WinCC Professional RT variant and vice versa. If a different PC runtime software is required, a licence matching the software must be purchased. The current order data can be viewed as usual in the Siemens Industry Mall. Notice: The procedure described in this article refers to the time at which this article was at the time of writing this article (status: May 2022). Your sincerelly, SIMATIC International Technical Support Hub |
Follow us on