(1)| 5/17/2022 3:40 PM | |
|
Joined: 3/14/2008 Last visit: 1/22/2026 Posts: 2233 Rating:
|
Hi, The Industry Library V9.0 is not compatible with PCS7 V9.1. But IL V9.0 SP1 is compatible. You need to upgrade to service pack 1 or you can install the newest version IL V9.1. You can quickly see which software is compatible in the online compatibility tool The Industry Library is not available free of charge. Minor updates can be downloaded from the support site, but service packs and base version must be purchased. |
Last edited by: Oreca at: 05/17/2022 15:43:45If I could help you, you can use the RATE button. Thank you. |
|
| 5/17/2022 5:12 PM | |
|
Joined: 3/14/2008 Last visit: 1/22/2026 Posts: 2233 Rating:
|
Hi, IL V9.1 can be ordered using the MLFB numbers in the following link: IL V9.1 You need to use the IL V9.0 SP1 installation, I don't believe there is a separate service pack for IL you can install, SP1 is a complete installation. I saw your attachment afterwards, is the AP library not installed? Can you show the installed software for your system? |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 5/18/2022 3:10 PM | |
|
Joined: 10/26/2011 Last visit: 1/23/2026 Posts: 766 Rating:
|
Hello Shuja Jani If you want to use IL V9.0 SP1 with PCS 7 V9.1 or PCS 7 V9.1 SP1, you have to fulfill the prerequisites, which are stored in the Compa Tool in the footnotes. See also my screenshot. |
|
SIMATIC PCS 7 - Overview |
|
| 5/19/2022 11:04 AM | |
|
Joined: 10/26/2011 Last visit: 1/23/2026 Posts: 766 Rating:
|
Something must have gone wrong. Please enter the article number, which you can find in the product note Sales and delivery release: SIMATIC PCS 7 Industry Library 9.1, directly into the search window/function of the Siemens Mall. |
Last edited by: Thunderstorm at: 05/19/2022 11:05:18SIMATIC PCS 7 - Overview |
|
Follow us on