(4)| 5/20/2022 8:57 AM | |
|
Joined: 2/17/2020 Last visit: 1/19/2026 Posts: 1251 Rating:
|
Hi 123Panda, After WinCC is installed, the WinCC OPC UA server can be used immediately without the need for any further configuration. However, please review this section of the communication manual: Configuring the WinCC OPC UA server On the other hand, remember that you need the Connectivity Pack license if WinCC is to act as an OPC server. It would also be important to check that the requirements detailed in the following FAQ are met: What are the requirements for operating OPC in connection with WinCC (V7 or Professional)? and finally, I would recommend you to try using OPC UA Expert as the TestClient. |
|
A rating will be well appreciated. |
|
This contribution was helpful to
|
|
| 5/20/2022 3:59 PM | |
|
Joined: 5/16/2016 Last visit: 9/24/2025 Posts: 42 Rating:
|
It's possible the issue is a windows setting. I attached a file from OPC Training Institute titled "OPC and DCOM: 5 things you need to know" which has helped me in the past. I advise you follow through the document and compare your setup. You can also check out the software from OPC Expert to help you troubleshoot. If anything these are great resources to have for living with OPC. AttachmentOPC and DCOM - 5 things you need to know - Windows 10.pdf (652 Downloads) |
|
Why you troubleshoot? |
|
| 5/24/2022 4:18 AM | |
|
Posts: 4 Rating:
|
Hi SilicornValley, Thanks for the info! Will check this one as well.
|
| 5/27/2022 8:33 AM | |
|
Joined: 9/3/2008 Last visit: 1/5/2026 Posts: 947 Rating:
|
Hi 123Panda The "OPC and DCOM ..." document will not help you as this only describes the Classic OPC which relies on Windows DCOM. It has nothing to do with OPC UA. These a two completely different technologies. |
|
Michael |
|
This contribution was helpful to
|
|
Follow us on