(0)| 5/31/2022 9:50 PM | |
|
Posts: 11 Rating:
|
hello ChristophD, I have the same problem: _the MC_Power function does not work, it only applies drive enable but not power enable + there is not any red LED ON on the Motormodules or on the SIMOTION D445 + HW information : D445-2 DP/PN, number: 6AU1 445-2AD00-0AA0, firmware: V5.3 + I use scout Tia V5.3.1.0 + LED States on the D445, the Infeed, and the motor Modules: green and orange, everything looks ok + I go online and check the drives with the control panel and the drives move with the TO control panel, from the TO control panel all the functions work well ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/01/2022 10:27:55New subject after splitting |
|
| 6/1/2022 5:02 AM | |
|
Joined: 5/12/2006 Last visit: 1/23/2026 Posts: 22831 Rating:
|
which infeed you use? Have you check that the Infeed ready signal was connected to the drives correctly? |
Follow us on