(0)| 11/3/2020 12:42 PM | |
|
Joined: 4/26/2016 Last visit: 1/21/2026 Posts: 47 Rating:
|
I have ET200S DP slave with 2AI i 2Wire Hs (6ES7 134-4GB50-0AB0) module in my s7-300 system. the module is now showing Fault. I need to replace the module. This module is obsolate and now 6es7 134-4GB52-0AB0 is available. i need to replace 6ES7 134-4GB50-0AB0 with 6ES7 134-4GB52-0AB0. While i am selecting "Replace object" in the SIMATIC Manager (v5.5) hardware configuration, it gives an erro "There is no replacement of this object" (HW Config (1230:5053). I don't want to change the program. i need to change the hardware only. Please suggest me how, i can change the faulty module with new module. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/04/2020 05:58:02New subject after splitting |
|
| 11/3/2020 1:34 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello VBP; The 6ES7134-4GB50-0AB0 module has been discontinued for some time now, and replaced by the 6ES7134-4GB51-0AB0. Now it looks like there is a successor module as direct replacement 6ES7134-4GB52-0AB0. But you software version cannot see it in the catalog. Possibly you might need Step 7 v5.6 to be able tp select it (I cannot fing a HSP to introduce it in an earlier version of Step 7). The critical word in the producrt description is "successor module), which means you couls still configure a 6ES7134-4GB50-0AB0 or even a 6ES7134-4GB51-0AB0 in your configuration, even if you have in reality a 6ES7134-4GB52-0AB0 in your rack. Look at this page of the 6ES7134-4GB52-0AB0 manual, showing the differences in performance of this module with its predecessor 6ES7134-4GB51-0AB0. https://support.industry.siemens.com/cs/ww/en/view/25240528/9446146827 Hope this helps, Daniel Chartier , |
| 11/4/2020 5:42 AM | |
|
Joined: 4/26/2016 Last visit: 1/21/2026 Posts: 47 Rating:
|
Dear Daniel, Thank you for your reply. You mean to say if i replace 6ES7134-4GB50-0AB0 module with 6ES7134-4GB52-0AB0 in the rack. It should work without change anything in the SIMATIC MANAGER software hardware configuration. I just replaced 6ES7134-4GB50-0AB0 with 6ES7134-4GB52-0AB0 in the PLC rack and without change hardware configuration and program, BF LED is blinking on the IM151-1 (151-1AA02-0AB0) and CPU 315-2DP and SF LED continuously glowing on the CPU 315-2DP. Note:- 2AI module 6ES7134-4GB52-0AB0 is listed in the catalog of V5.5 +SP3 installed in my computer. I tried with manually delete 6ES7134-4GB50-0AB0 (PIW 306-309) and add 6ES7134-4GB52-0AB0 (PIW306-309). But while hardware compilation, it gives an error The "2AI I 2WIRE HS" module cannot be configured in this rack (slot 8 in rack with PROFIBUS address 4, DP master system_1) The system data could not be recreated because the configuration is inconsistent. If i change back to 6ES7134-4GB50-0AB0, it compiles ok. The configuration file is attached. Thanks Vishnu Attachmentstation simatic 300.zip (785 Downloads) |
Last edited by: VBP at: 11/04/2020 05:44:57Last edited by: VBP at: 11/04/2020 06:44:35Last edited by: VBP at: 11/04/2020 06:49:18 |
|
Follow us on