(0)| 7/31/2022 6:35 AM | |
|
Posts: 96 Rating:
|
Dear Sir, I have 400H CPU & two PC(One ES & One OS) fitted with dual CP1613 Cards, Do ,I have to integrate my WINCC project in Step 7 or I can do separate Wincc project to achieve fault-tolerant redundant communications of PC's with H-CPU If possible ,Can I Get the configuration procedure. Thanks & Regards, Samir
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/01/2022 10:59:28New subject after splitting |
|
| 8/4/2022 9:55 AM | |
|
Joined: 8/3/2009 Last visit: 1/20/2026 Posts: 16644 Rating:
|
Hello SAMIRKM I think you have to go with: http://support.automation.siemens.com/WW/view/en/16667714 and S7 Redconnect and integration in Step7 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on