(1)| 8/4/2022 11:11 AM | |
|
Joined: 5/3/2017 Last visit: 12/5/2025 Posts: 673 Rating:
|
Hi citizen_2222, in the general the virtualization of your system without upgrading the PCS 7 version is possible. But you have to consider the number of fault-tolerant connection with the Standard Ethernet network adapter is limited to 4 with a single ring. A network topology with two rings is not possible and you need two additional licenses (see the manual Fault-tolerant Process Control Systems at the section Connecting PC stations to the plant bus)
The best way to virtualization a existing system is with programs that scans your IPC or computer and create a VM. Then you have all settings, programs and licences keys already in your VM. With regards |
Follow us on