(0)| 8/2/2022 2:59 PM | |
|
Joined: 3/7/2011 Last visit: 12/5/2025 Posts: 7 Rating:
|
Hello, I have the same problem with a TP1200. We took out the scalance and made a direct connection between the HMI and the CPU. The error LED on the CPU is only on when I pull the cable out otherwise the LED is off. The only way to restore it is to restart the screen by taking of the supply. Here is also the diagnostic file of the CPU. The errors you see on 8/02/2022 are the tests we did. There are no other faults and that while the HMI had the problem earlier that morning. If somme one has the answer to this problem I'l be glad to hear it. ------------------------------------------------------------------------------------------ AttachmentDiagnostics2022082.txt (186 Downloads) |
Last edited by: Jen_Moderator at: 08/03/2022 09:46:47New subject after splitting |
|
Follow us on