8/15/2022 8:01 PM | |
Joined: 3/3/2015 Last visit: 8/7/2025 Posts: 9 Rating:
|
Hello, I have exact the same problem. I use TIA Portal Step7 Professional V17, the harwdare is a CPU 1507S (6ES7 672-7AC01-0YA0) Software version V21.9. It runs at an cycle of 1 - 2 ms The biggest problem of the S_Move is at this moment in my project that it is not relaible because of the EN / ENO. If I set EN it takes 1 scan and the ENO is hight BUT 99/100 times it does not move the value (STRING in my part 32 bytes long). As test i used a timer and after 150ms or so the value is moved. So i made an instruction to enable the S_Move and if value A is the same as B i stop moving and i do the rest.. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/16/2022 08:24:55New subject after splitting |
|
Follow us on