(0)| 8/23/2022 9:17 AM | |
|
Joined: 10/16/2020 Last visit: 1/14/2026 Posts: 146 Rating:
|
Hi, Windows 11 is not yet released for many versions of Siemens software. In this case, WinCC Advanced v15 is not found in the compatibility excel. You can use the Kompatool to check it. I would recommend you to use a VM with an OS that is released. BR. Cookie_M0nster |
|
If this information has been helpful to you, please don't forget to rate it. |
|
| 8/29/2022 8:40 AM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello Pryjanko Its not 100% clear whats your problem out of your description... If you want to run a WinCC advanced Runtime Application then you also have to create a WinCC advanced Runtime in your TIA Project, no KTP Panel. Second one is, that the Transfer to a Advanced RT can be done online like on a Panel with Runtime loader (loading the Runtime files automatically from TIA Portal to the Runtime PC) Or offline. If you do it offline then use the following FAQ to get all the needed files coppied to the Runtiem PC. Only the fwx file is not all you would probably need: https://support.industry.siemens.com/cs/de/en/view/109740696 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on