(0)| 5/11/2021 4:45 AM | |
|
Posts: 1 Rating:
|
Dear all, I have a problem with SFC type faceplate where the some parts(picture window) are not scale properly which make operation of SFC type impossible. I play around with the '@pg_@sfc_type.pdl' and its component for several days and can't figure it out. This problem, I believe, is caused by resizing the OS project to 4k resolution to match with customer's requirement. The other objects and faceplates from APL are scaled correctly and working fine. If anyone have recommendation, please help me out. Version: PCS7 V9.0 SP3 Library APL V9.0
AttachmentFaceplate Resizing.zip (419 Downloads) |
| 5/11/2021 6:48 AM | |
|
Posts: 198 Rating:
|
Hello Slurbee, If my understanding is right, the truncation of SFC faceplates happens only after the OS project editor resolution change and until then the SFC faceplates were fine? If this is the case, it looks like a potential SFC Visualization issue where you might get better assistance with a Technical Support Request as there is limited troubleshooting to perform in this case. Technical Support Request Link Hope this helps |
This contribution was helpful to
|
|
| 9/2/2022 2:13 PM | |
|
Posts: 14 Rating:
|
Hi I'm having the same problem does your problem solved? |
Follow us on