(0)| 9/12/2022 1:18 PM | |
|
Joined: 12/13/2014 Last visit: 1/13/2026 Posts: 157 Rating:
|
You can do it with LOGO. Safety circuits are a separate topic anyway (safety relays, safety contactors, etc.) What you want is to control the welding machine and display an error message.This is a task that LOGO can handle. You need a timer and an AND logic element as a minimum. Even better is an RS trigger, so that resetting the machine error state is a separate operation (via separate input for example). Example for start. I didn't really understand where and how the sensor works (connects/disconnects circuit?), so I left it out of the schematic for now. Adding sensor circuit is not a big problem either. AttachmentWeldingMach_V1.zip (447 Downloads) |
Last edited by: WWEE at: 09/12/2022 13:43:20Last edited by: WWEE at: 09/12/2022 13:51:36 |
|
Follow us on