(0)| 1/13/2021 1:19 PM | |
|
Posts: 114 Rating:
|
Hello Siemens EXPERTS SCADA -WINCC 7.5 SP1 (Both scada are standalone) HMI-(6AV21240QC020AX1) PLC- 6ES74125HK060AB0 SCADA SYSTEM IS STANDALONE HMI IS STAND ALONE Is is neccessary to take CP 1612 & Redconnect IN S7-400H ? if Not Then How to Connect two 400 H Plc to Wincc ? How to Give S7-Connection In wincc Named Connection ? Is there any Configuration Manual Available with IE GENERAL Card? I am Attaching System Architecture.........................!!!!!!!!!!!!!!!!!!!!!!!!!! Attachmentsystem_arch.pdf (269 Downloads) |
Last edited by: vicky bhau at: 01/15/2021 07:00:30 |
|
| 1/15/2021 2:01 PM | |
|
Posts: 7298 Rating:
|
Hello vicky bhau, a CP 1612 can not be used for named connection, it is Fault-tolerant S7 connections are available only for CP1613 see the FAQ: https://support.industry.siemens.com/cs/ww/en/view/16667714
Georg Berghof |
| 9/8/2022 10:18 AM | |
|
Posts: 19 Rating:
|
CAN I USE CP1628 |
Follow us on