(2)| 9/15/2022 9:37 AM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hi, When you go to hold in a specific step and after resuming, you go back to the same step, then Initialization is not executed, only the Processing. I'm pretty sure if you activate a target step, so after resuming the SFC goes to the target step you defined, then Initialization is executed because it's a new step. PS: We are using EPHT and EMT with technological commands. The supplied CmdStatLib library (default in SFC library) is not good. For example, commands like ShowPositionText are only executed in Initialization. If we go back from hold to the run step, the command is not executed anymore. We have changed all commands to Processing. Also command like StartTimer is changed. When a timer was started in an active step and the SFC goes to hold and back to active step after resuming, the timer was not executed anymore because only Processing is executed.
|
Last edited by: Oreca at: 09/15/2022 09:40:20If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
Follow us on