9/1/2022 5:15 PM | |
Joined: 1/7/2022 Last visit: 3/28/2024 Posts: 9 Rating:
|
Hi We are using PCS7 v9.0. v3 and we have this system fault about device coming and going all day. Thanks |
9/2/2022 11:24 AM | |
Joined: 9/9/2015 Last visit: 4/9/2025 Posts: 732 Rating:
|
Hi Urai, Can you do the below steps and show us few screenshots? (monitoring on the block and block properties) 1. Simatic manager-> component view 2. under AS user project, S7_program folder (AS2_Program) 3. Click the Chart , Sort by Name, look for "@(10)" 4. Look for block name "330-PP-001R_1" 5. test mode on -> Watch on the block, add I/O to all I/O. 6. take one picture. 7. Then , double click the block, open up the block properties, take one picture. 8. Then back to component view -> block folder -> record down the block version, and date here. 9. Take a picture on the hardware configuration on this device as well, and its gsd properties. (Normally, PCS 7 Basis library upgrade will resolve this kind of abnormal issue. Hope this is helpful.
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
1 thankful Users |
9/9/2022 12:04 PM | |
Joined: 1/7/2022 Last visit: 3/28/2024 Posts: 9 Rating:
|
I was wondering if i can configure into special properties "Messages" take off SIG8.
AttachmentScreenshots.zip (455 Downloads) |
Last edited by: The Helping Hand at: 09/09/2022 12:15:45Zipped all screenshots Last edited by: The Helping Hand at: 09/09/2022 12:17:10 |
|
Follow us on