(0)| 9/27/2022 12:11 PM | |
|
Joined: 2/17/2020 Last visit: 1/21/2026 Posts: 1251 Rating:
|
Hi, Have you followed in detail the migration example from the initial version (V6.X) to the current one (V7.4)? How do you migrate WinCC projects to new versions of WinCC from V4 to V7? Although it is working correctly (except for the archive data), it may be interesting to review the migration process. On the other hand, note that if you have redundant WinCC servers, when the files of both servers are copied to the 'Common archiving' folder from the same time period, then you get the information "NoAttach" for the files of the timeperiod which is already attached. Other situation where "NoAttach" can occur are if the files are read only or defective, or there are problems with the permissions. Hope this narrows down the problem a bit! |
Last edited by: itafusna at: 09/27/2022 12:12:19A rating will be well appreciated. |
|
Follow us on