10/17/2022 1:38 PM | |
Joined: 9/6/2022 Last visit: 7/12/2023 Posts: 1 Rating:
|
Hello, I'm learning to work with SIMATIC RF1070R. I'm able to communicate with the reader and control it, but I have issues with syscmd_reset. The request I send to the reader is 0C 00 C3 00 00 00 and it is exactly like the one in the manual (https://cache.industry.siemens.com/dl/files/625/109780625/att_1032797/v1/109780625_RF1070R_CM1241_ReadUID_DOCU_V10_en.pdf). The problem is I get 8C 00 C3 01 00 41 in response (response without error should be 0C 00 C3 00 00 00) and I can't find anything about his error. Can anyone tell me what this error means and how to prevent it? Thank you for your help. Attachment109780625_RF1070R_CM1241_ReadUID_DOCU_V10_en.pdf (908 Downloads) |
Last edited by: Jen_Moderator at: 10/18/2022 08:26:59PDF added from link. |
|
Follow us on