(0)| 10/18/2022 11:28 AM | |
|
Joined: 7/2/2015 Last visit: 11/13/2025 Posts: 96 Rating:
|
Hi Kalafony, Access to WinCC databases is encrypted and you need one of the paid options to access them: Connectivity Pack, Information Server or Industrial Data Bridge. The connectivity pack you have to program everything, let's say it gives you the drivers to decrypt it, but you have to program everything. If we make a simile of cooking, I would give you the ingredients. The Industrial Data Bridge is an application independent of the engineering or runtime software that provides you with data in certain formats. If we continue with the simile of cooking, I would give you the cooked ingredients. You just have to plate them. And finally, the Information Server generates the information for you, already with formats. That is, going back to the simile of the kitchen, it gives you everything already on a plate. From the Industrial data Bridge, you can find the example: "WinCC/IndustrialDataBridge: Writing data from SIMATIC WinCC or from SIMATIC controllers in MS Office files": For the Information server, you can follow the example: "Creation of report templates for the Information Server based on Process Historian data in the WinCC and PCS 7 Environment": Finally for the Connectivity Pack, you can follow this example: "Exporting Archive Data with the Aid of the SIMATIC WinCC/Connectivity Pack (OLE DB Provider)": |
Last edited by: Jen_Moderator at: 10/18/2022 11:52:50Text formatting optimized. If this Information really helps, you could use the Rate function |
|
Follow us on