10/25/2022 6:38 AM | |
Joined: 5/3/2017 Last visit: 2/6/2025 Posts: 673 Rating:
|
Hi Farah_Fuad, in the attachment you can find an introduction and the source code for transfer from the PLC date and time to WinCC. With regards AttachmentDT_to_WinCC.zip (439 Downloads) |
This contribution was helpful to
2 thankful Users |
10/26/2022 7:18 AM | |
Joined: 5/3/2017 Last visit: 2/6/2025 Posts: 673 Rating:
|
Hi Farah_Fuad, if you want to create a Block with SCL you can not do it in the folder blocks instead you have to do it in the "Sources"-folder. All other addition information about SCL can be found in the manual S7-SCL V5.3 für S7-300/400. With regards |
10/26/2022 11:17 AM | |
Joined: 9/15/2019 Last visit: 1/28/2023 Posts: 10 Rating:
|
Thank you. I tried the function and it works perfectly. Any idea how I can save the these date and time values in the tag management? |
11/3/2022 1:49 PM | |
Joined: 1/11/2019 Last visit: 8/14/2025 Posts: 899 Rating:
|
Hello Farah,Heisenberg2 has already given the complete instruction in his first reply. Kindly go through it |
Follow us on