(0)| 11/11/2022 4:11 PM | |
|
Posts: 2 Rating:
|
And what to do if the panel does not have USB? I am dealing with a TP177A. The screen is broken, I can see less than half of the screen working, and the touch is not working either. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/14/2022 08:13:45New subject after splitting |
|
| 11/14/2022 7:29 AM | |
|
Joined: 8/3/2009 Last visit: 1/20/2026 Posts: 16653 Rating:
|
Hello juan_fernandez_uy Then you cannot connect a Mouse. -> so you cannot control the panel anymore. You only have the chance if the automatic transfer is activated to do a Backup with SIMATIC Prosave. LINK Then you have to change the Panel (Repair Center or Sparepart) Then you can do a restore or transfer the project if you have the WInCC flexible project Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on