(0)| 1/30/2017 2:51 PM | |
|
Joined: 4/9/2010 Last visit: 7/4/2025 Posts: 236 Rating:
|
Hello, I'd like to replace a CPU 1211C FW 3.0 with AS-i module attached to it with CPU 1214C FW 4.1 but I get an error during compilation: CPU firmware versions V4.0 and higher are not supported. Use a CPU V3.x. Is there a way to make the two compatible? Please help. Thanks, Adam -------------------------------------------------------- Update for 2017-02-01 FAQ was posted yesterday regarding firmware update for this module but I can't find the file to download. --------------------------------------------------------- Update for 2017-02-06 Got the file from Technical Support. Problem solved! |
Last edited by: adam_ski at: 1/30/2017 2:51:42 PMLast edited by: adam_ski at: 2/1/2017 2:01:50 PMLast edited by: adam_ski at: 2/6/2017 2:17:05 PM |
|
| 6/10/2020 8:06 PM | |
|
Joined: 12/18/2018 Last visit: 11/27/2024 Posts: 2 Rating:
|
Hello, I see the question was asked 3 years ago, but I am answering it regardless. Maybe someone will find it useful in the future. The AS-i CM 1243-2 FW 1.0 module only works with S7-1200 FW 3.x. Above 4.0 it will give an error in TIA Portal. So you must updrate the firmware of the CM 1243-2 module above 1.1. You can find the required files here: https://support.industry.siemens.com/cs/document/109759715/firmware-update-for-cm-1243-2?dti=0&lc=en-WW. Some help for how to do the update: https://support.industry.siemens.com/cs/document/109744251/how-do-you-update-the-firmware-of-the-as-interface-master-cm-1243-2cm-1243-2-communication-module-?dti=0&lc=en-WW If you have TIA Portal you can also start the update on the Online & Diagnostics/Functions/Firmware update page of the module. |
This contribution was helpful to
|
|
| 11/18/2022 8:08 AM | |
|
Posts: 8171 Rating:
|
New question published by Paulh07 is split to a separate thread with the subject The check box in the Tia Portal to activate de FW after start de upgrade does not work. Best regards |
Follow us on