(0)| 11/16/2022 3:39 PM | |
|
Joined: 5/30/2022 Last visit: 1/19/2026 Posts: 634 Rating:
|
Hi Dung922, Check this example which is valid for what you are asking for as it is Visual Script: How do you implement a wait function (delay) in a Visual Basic script in WinCC flexible? |
|
If this information really helps, you could use the Rate function. |
|
| 11/18/2022 1:01 PM | |
|
Joined: 8/3/2009 Last visit: 1/19/2026 Posts: 16644 Rating:
|
Hello Dung922 I suppose you use WInCC Professinoal RT -> Here you can also use a synchronus writing, with this your script waits until the value is written into the PLC with a feedback. The same you can do with reading here a few information about an an example in the help system: https://support.industry.siemens.com/cs/ww/en/view/109798671/36120923147 This should be a better option than using a wait/sleep function Bye Murof |
Last edited by: Murof at: 11/18/2022 13:03:07If this Information really helps, you could use the Rate function |
|
Follow us on