(0)| 4/28/2022 6:38 PM | |
|
Posts: 5 Rating:
|
Hi, In this sample project only the "static" faceplates scale in function off the screen size. Is it possible to scale popup faceplates in function of the screen size as well? I have a button inside a static faceplate. When pressed, another faceplate opens in popup. Although I use the parent width and height (See attachment "Script_call_popup"). The popup faceplate does not scale in function of the screen size. the static parent faceplate does scale. The other two attachments show the popup faceplates in full screen mode and with a smaller resolution. In both cases the scaling of the popup faceplates are identical. ------------------------------------------------------------------------------------------ AttachmentAttachments.zip (513 Downloads) |
Last edited by: Jen_Moderator at: 04/29/2022 10:05:04New subject after splitting |
|
Follow us on