(1)| 11/26/2022 4:32 PM | |
|
Joined: 9/23/2005 Last visit: 1/22/2026 Posts: 4451 Rating:
|
Hi, WinCC Unified V18 is now available for download (https://support.industry.siemens.com/cs/br/en/view/109807109), but during installation it is not possible to select the option to simulate HMI. This is because the simulation has to be downloaded and installed separately (https://support.industry.siemens.com/cs/br/en/view/109814516), e.g. after the WinCC Unified ES installation. The no installation of the runtime package together with old TIA versions can lead to the following error message when trying to start the simulation: "An incorrect runtime version is installed. The installed runtime cannot process the project. Install the runtime manually on the target device". |
Last edited by: Denilson Pegaia at: 11/28/2022 20:45:03Denilson Pegaia |
|
This contribution was helpful to
|
|
Follow us on