(2)| 11/30/2022 2:13 PM | |
|
Joined: 9/23/2005 Last visit: 1/16/2026 Posts: 4449 Rating:
|
Hi As TIA V18 it is possible to perform a frequency dominium analysis of a traced signal, using the Fast Fourier Transfer and the Bode Diagram To create a Fast Fourier Transfer Diagram:
The body diagram represents amplitude and phase relationship between two signals. TIP: the FFT need that the analyzed variable would be sampled at constant time interval (that means it should be linked to a cyclic time interrupt OB – no Main OB). Sample project AttachmentProject5.zip (620 Downloads) |
|
Denilson Pegaia |
|
This contribution was helpful to
|
|
Follow us on