(0)| 1/12/2023 10:39 AM | |
|
Posts: 41 Rating:
|
I would like to configure a MP370 panel as OPC server. For a test, I have installed the example application that I have find here: What options are there in WinCC flexible for using a Multi Panel or Mobile Panel a... - ID: 22701694 - Industry Support Siemens I can transfer and run it in the panel, but when I try to connect from a OPC explorer in a computer, in the panel I see the following error: Simatic WinCC Flexible 2008 SP3 Runtime: License key not available! Simatic WiCC Flexible /OPC-Server for Simatic Multi Panel. From WinCC Flexible 2008, in project --> transfer --> license keys I have the license for WinCC Flexible /OPC-Server for MP's v1.5. I think it is the correct license, but I am not sure. What I would like to do it is to can run the example proyect and connect with a OPC XML explorer to read the items of the application. |
| 1/12/2023 1:25 PM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject How to configura the OPC server in a MP370 panel? is published within the conference SIMATIC WinCC flexible. Jen_Moderator |
Follow us on