(0)| 1/3/2023 7:51 AM | |
|
Joined: 1/16/2012 Last visit: 6/30/2025 Posts: 127 Rating:
|
Dear Experts, I have WinCC installed and it is running fine with all PLCs that are communicating through PROFIBUS via IE/PB module with the WinCC server. Now I want to add one new PLC that is CPU 314C-2 PN/DP installed in rack # 0 slot # 2 and configured in TIA V16. I have set up the TCP/IP driver in WinCC and used the same IP, rack, and slot but the communication is not getting up. The IP address I can ping from the WinCC server. Please support resolving the issue. Best regards, Tech Ahmed AttachmentIssue Snap.zip (428 Downloads) |
Follow us on