(0)| 1/18/2023 3:50 PM | |
|
Joined: 3/10/2016 Last visit: 10/26/2025 Posts: 4 Rating:
|
Dear All, I am facing difficulty in loading archive backup of a CNC machine from PCU50 to SINUMERIK 840D to SIMODRIVE 611. I have regenerated the HDD via OEM provided backup/ghost image. I am loading archive with following steps 1. Go to Startup change the level to machine manufacturer 2. Go to Service -> Data In-> select the required archive-> Start transferring the archive. When I load PLC archive it's normal but as soon as I try to load NC archive it ends up with errors Attached are the snapshots of the errors. as soon as archive reaches "\DG\MDDRV\DRV1.TEA" error list shows errors and continue errors for all 5 drives. Looking forward for some solution. ------------------------------------------------------------------------------------------ AttachmentError_Details.zip (481 Downloads) |
Last edited by: Enghineer_S@LM@N at: 01/18/2023 16:07:58Last edited by: Enghineer_S@LM@N at: 01/18/2023 16:09:05Last edited by: Jen_Moderator at: 01/19/2023 09:44:53New subject after splitting |
|
Follow us on