1/15/2023 3:38 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Yes. |
1/15/2023 5:10 AM | |
Joined: 10/17/2007 Last visit: 9/12/2025 Posts: 4449 Rating:
|
See the infeed module basic drawing . T. 72 is a NO contact of small relay. --if you checked all enabling and you all drives are no problem (drive status transfer back to infeed from device bus) --your yellow LED on ,your green LED off?--- if everything ok as you said it is possible that small relay has issue. I suggest --NOT replace control card for Infeed (it is not like drive--card and power section removable ) --you need replace the whole infeed module to trouble shooting --then send bad module to repair shop the infeed module version A,B or C will compatible if power rating same
AttachmentInfeed Module basic drawing.pdf (954 Downloads) |
If you like my comments please |
|
This contribution was helpful to
1 thankful Users |
Follow us on