(0)| 1/30/2023 4:17 AM | |
|
Joined: 6/15/2016 Last visit: 9/5/2025 Posts: 12 Rating:
|
Hi Bari, Need your help in fixing below problem. I am having a host laptop and a Hyper-V vm. PLC SIM in host and WinCC 7.5 in the vm. Communication between PLC and WinCC is over TCP/ IP and its working fine when connected physically as well as in simulation when both run in the host. But, when I try to run WinCC from vm communication is not getting established with PLC sim running in host. Br, Zakir Sayed ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/06/2023 13:23:02New subject after splitting |
|
Follow us on