(0)| 2/8/2023 4:55 PM | |
|
Posts: 5 Rating:
|
Dear Experts, I need your help. I use WinCC V7.4 ( redundant servers ) and GE protection relays (G60, T60, G30, L30, and 345). Reporting doesn't work while polling works. I imported tags from CID.file following instructions from WinCC IEC61850 Documentation_general.pdf. In the attachment, you can see the connection parameters that I choose. I also tried to capture the communication between some protection relays and the Master Server. As you can see in the attachment there is an error that says the object is non-existent. Did anyone have the same problem? BR, JMV ------------------------------------------------------------------------------------------ Attachmentpic.zip (288 Downloads) |
Last edited by: Jen_Moderator at: 02/09/2023 10:41:46New subject after splitting |
|
Follow us on