2/21/2023 6:42 PM | |
Joined: 3/28/2010 Last visit: 9/26/2025 Posts: 1177 Rating:
|
There is the possibility of outright bad firmware in the slave that outputs null characters for reasons likely unknown to whomever it was that programmed it. But, why would the slave work with a one master and not another? Why would it output a couple null characters when connected to one device but not when connected to another device. The failsafe biasing is accomplished by the connection from the 485 driver lines to a pull-up resistor to the RS-485 5V supply line and a pull-down resistor to the DC common/ground. Lunar phase |
This contribution was helpful to
1 thankful Users |
Follow us on