2/28/2023 6:21 AM | |
Joined: 7/26/2008 Last visit: 9/16/2025 Posts: 109 Rating:
|
Hi Kiiza, SIMATIC manager ( Step 7 V5.6 SP1 + HF1) has a good example in the help function. Go to Step 7 -> Help -> Help on STL -> Example of Memory Indirect Addressing. I attach a source file with a function that will populate a DB with 100 Real values from 100.0 to 1.0. This function can easily be adapted to your requirements. The function is close to the example however. The basic process is to initialize the Loop index, calculate a value (which can include the index) and then write the calculated value to the DB indirectly in each loop. Good luck! AttachmentPopulate.txt (630 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on