(0)| 5/18/2009 1:30 PM | |
|
Posts: 419 Rating:
|
Hi The problem is that the Siemens SIMATIC S5 PLCs are programmed via a TTY serial interface (called also 20mA Current Loop). To connect a PC, which is normally equiped with RS232 ports, a converter is therefore required. You can try to find one on the internet or you can try to bild you one. I send you one which I found it on a site but it is a passive one. I don't know if it is working but I think that is worth to try it. Good luck Nit Attachment232_20MA.zip (629 Downloads) |
| 5/18/2009 3:16 PM | |
|
Posts: 9 Rating:
|
Hi Thanks for your reply, My system is a SINUMERIK 840C Controller, with integrated S5 PLC . |
| 5/18/2009 4:20 PM | |
|
Joined: 11/25/2005 Last visit: 11/26/2025 Posts: 21 Rating:
|
HI, It is possible to communicate with the S5 plc of 840C with a pc equipped of a serial port. Here is the drawing of the cable, kept from Doc on CD 840C ( given for a 25 poles serial port). Regards Attachment6FC9 344-4R.pdf (683 Downloads) |
Follow us on