3/7/2023 6:16 AM | |
Joined: 1/21/2013 Last visit: 11/14/2024 Posts: 3271 Rating: (508) |
Hi MartinHM, WinAC RTX only supports the 32-bit variants of Microsoft Windows XP Professional SP2 and SP3 or Microsoft Windows 7 Ultimate, Professional and Enterprise (see system requirements). Windows Embedded Standard 7 like available for SIMATIC IPC477E is also supported. This is because it uses IntervalZero RTX 2009, which is itself limited to these systems. So you must use a SIMATIC IPC477E with Windows Embedded Standard 7. Kind regards |
Follow us on