3/11/2023 5:58 PM | |
Joined: 3/28/2015 Last visit: 9/14/2025 Posts: 725 Rating:
|
Hello, Perhaps the following summary from the manual might help: 6ES7 334-0CE01-0AA0 1- Not parameterize, setting of measurement and output type by means of wiring. 2- Measuring range of 0 to 10 V or 0 to 20 mA 3- Output range of 0 to 10 V or 0 to 20 mA 4- Select the measuring method of an input channel (voltage, current) by wiring the input channel appropriately.Select the type of output of an output channel (voltage, current) by wiring the output channel appropriately.
|
Eng.Mohamed Ibrahim |
|
Follow us on