(0)| 3/7/2023 10:18 AM | |
|
Joined: 2/17/2020 Last visit: 1/19/2026 Posts: 1251 Rating:
|
Hi, The problem here can arise when accessing the OS (or ES) that has server services, such as a server OS or also a client OS that acts, for example, as a WebNavigator or WebUX server. If you use a non-released remote access to access this type of OS, it is possible that you will "throw down" the server services that WinCC has on this computer, causing stability, communication problems, etc. It is also possible that it works without problems for years, but the fact is that it could not be guaranteed. According to the FAQ with ID 78463889, the only application released to remotely access this type of OS PCs is RealVNC, so I would recommend using only this one. With OS that do not have server services, such as a basic client OS, this problem does not exist so in principle any remote access can be used: RDP, UltraVNC, etc. I hope I have clarified the subject a little! |
|
A rating will be well appreciated. |
|
| 3/11/2023 8:19 PM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hi mark, Correct, UltraVNC V1.3.8.1 is released for PCS7 V9.1 SP2 |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
Follow us on