3/13/2023 12:28 PM | |
Joined: 12/16/2021 Last visit: 8/22/2023 Posts: 126 Rating:
|
Hi Autogen_7948938 Connect the motor or check the motor contactor. ( remedy for error code 7410 ). 1. Check the motor parameterization and the connection type (star-delta). 2. Check the DC link voltage (r0070). 3. Check the power unit. 4. Activate the "flying restart" function (p1200). and please check back this post here
|
If The Information Helpful, Then Don't Forget Give (To thank ) and Rate It |
|
Follow us on