3/21/2023 9:43 AM | |
Joined: 1/30/2015 Last visit: 4/3/2025 Posts: 4 Rating:
|
Hi All, I have an SF fault on a processor that I am unsure how to rectify. The attached Diagnostic file is attached. This system has around 20 profibus nodes that when the power is cycled they take a while to come back onto the network therefore in the log events 1 to 26 are related to that. Event 31 is related to the 2nd ethernet port on the processor which is not currently plugged in - as OB82 can not be found I'm thinking this is the problem. There are lots of faults showing P area, word access, Access address: 320 Address 320 is related to a FM350-1 counter module. If someone could point me in the right direction that would be great. AttachmentDiagnostics File.txt (597 Downloads) |
3/21/2023 11:19 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, Distributed IO module with input address 2045 is failed. Please check. |
Follow us on