(2)| 12/13/2011 3:15 PM | |
|
Joined: 10/3/2010 Last visit: 1/14/2026 Posts: 1572 Rating:
|
check the attached sampleAttachmentTagInfo Behind Object Example.pdf (1849 Downloads) |
|
B r g d s , |
|
| 12/14/2011 4:47 AM | |
|
Joined: 12/27/2007 Last visit: 5/29/2025 Posts: 80 Rating:
|
Hi, Thanks for the reply. Can you please suggest VB script.Customer insist use of VB script only. Regards, |
| 12/14/2011 7:23 AM | |
|
Joined: 10/3/2010 Last visit: 1/14/2026 Posts: 1572 Rating:
|
Tell your customer that chosing WinCC also means that some functions are only possible with C scripts and others only with VBS. I'm not sure but as far as I've read here, this one's only available in C. Another option is to use Text Reference tags (see WinCC manuals) where each Text Reference tag refers to unique ID in the Text Library. It's quite some work but in the end, it's another solution. It means you have to enter all Addresses in the Text Library and write down there ID. That ID is the start value of the referring Text Reference tag. Value of those Text Reference tags can be called by VB-script. |
|
B r g d s , |
|
| 12/14/2011 11:06 AM | |
|
Joined: 12/27/2007 Last visit: 5/29/2025 Posts: 80 Rating:
|
Thanks Aidan, Please see attachment. My requirement was to get the Popup to change the setpoint value by clicking on I/O field. Ihave achieve this , but not sure about is it the best practice.. Thanks again AttachmentPopup Up to Change the Setpoint.pdf (1098 Downloads) |
This contribution was helpful to
|
|
Follow us on