(0)| 3/28/2023 10:13 AM | |
|
Joined: 3/30/2020 Last visit: 1/22/2026 Posts: 5675 Rating:
|
@cliff.pennalligen: Brilliant write up.
@ABD.HAS00: I am assuming that the on/off pulse frequency generated by the PLC is too slow. The inductance of the motor does not "smooth out" the current enough. The motor "sees" an on/off pulse. The best solution would be to use a driver (H-bridge). A inductor based low pass filter (https://industrial.panasonic.com/ww/ss/technical/b4) may also work -- but I am still concerned about using the PLC outputs directly. |
|
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on