3/30/2023 9:13 AM | |
Joined: 7/3/2015 Last visit: 7/31/2023 Posts: 1 Rating:
|
Hi, I am testing different animation options in WinCC Unified V18. Using Custom Web Controls, I alredy tried: 1. Animated svg files -> works fine 2. Objects animated with CSS animation, transform, translate, key frames -> works fine 3. Objects moving along the path, animated with gsap. And it does not work. Well, it works in the normal web browser, but not in WinCC. All objects are created, but there is no movement. Does anyone have a similar issues.... I do not know if it is a matter of gsap in webCC, but isn't webCC just buit for that purpose exactly - to let web html/js engine do the job instead of WinCC ... Attachment is the zip to include in MyControls (UserFiles) or unzip and run in browser Paweł Kolon Attachment{551BF148-2F0D-4293-99C2-C9C3A1A6A096}.zip (292 Downloads) |
Follow us on