(0)| 4/1/2023 5:50 PM | |
|
Joined: 10/31/2021 Last visit: 2/15/2025 Posts: 4 Rating:
|
Hello, this topic is the continuation of : S7-1200-CM1241-RS485 Modbus RTU problem The manufacturer send me a new cables to connect to the rectifier to control. Now I can use Modbus RTU and I am still a bit stuck of ho to do it. I am attaching the documents for control of Modbus RTU. I see how to read the holding registers , but I cannot see how to write to them. There are some commands: Register read command: Read Holding Register 0x03 But I only know how to read and write by modifying the Mode parameter in MB_MASTER. What could these commands be? I need to send voltage and time for control and I need to read the voltage, current, time and errors. Can somebody help me with this connection? Thank you AttachmentProtocollo di Comunicazione RTU RCV EN R1.0.pdf (1044 Downloads) |
Follow us on