(0)| 4/20/2023 8:26 AM | |
|
Joined: 8/3/2009 Last visit: 1/21/2026 Posts: 16653 Rating:
|
Hello EduardoFS I think I remember that there was a bug in the early version. Install the latest Update for TIA V17: https://support.industry.siemens.com/cs/ww/en/view/109784441 then check if you have set the device to the V17.0.0.0 in the project -> then install the latest Panel image Package for V17: https://support.industry.siemens.com/cs/de/en/view/109746530 Then do a OS Update to the latest V17 Image Then try again, even after the Upd in TIA the Simulation should work OK and after the Image Update also the Panel should not birng up the message again (Or of course you would use an older Image Version in TIA but this is not a nice solution) Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on