(0)| 3/26/2023 5:16 PM | |
|
Posts: 4 Rating:
|
Hello, I am configuring SiVArc to create an animation for my plant. In one station the colors must be determined by a variable of the block. I am a bit new to this so please forgive me if I missed some fundamentals but I could not find much information about this. (Only this) SiVArc must recognize where it is (at which block) since I am using multi-instance and provide as input of the animation tag, an static variable of the FB. Lets assume the Block has a signature like this: Static -> MyBoolVariable First "assumption": I defined the animation with a dummy variable hoping that SiVArc replaces it with the tag specified: Second "issue": I have tried the following references to use my tag but none of them work:
PS: I used this as reference but I was unable to find a complete list of "keywords" for example I can find Block.Parameters("Tag name").Value, but I am not sure how to address the actual variable, not the value. Thank you in advance Regards |
| 4/17/2023 10:38 AM | |
|
Posts: 1086 Rating:
|
Hello AppData, if you need help, you should post basic information: |
This contribution was helpful to
|
|
Follow us on