(0)| 4/27/2023 6:06 PM | |
|
Posts: 1 Rating:
|
I'm accessing the router CLI/SSH, but I can't change the switchport field to dedicated routing Mode. Follow the command line below: login as: admin admin@192.168.1.2'spassword: Welcome to Rugged CLI admin connected from 192.168.1.10 using ssh on ruggedcom ruggedcom# config private Entering configuration mode private ruggedcom(config)# interface ruggedcom(config-interface)# switch lm2 1 ruggedcom(config-switch-lm2/1)# ruggedcom(config-switch-lm2/1)# switchport Possible completions <cr> ruggedcom(config-switch-lm2/1)# switchport Possible completions <cr> ruggedcom(config-switch-lm2/1)# switchport ruggedcom(config-switch-lm2/1)# disable --------------------------------^ syntax error: unknown command ruggedcom(config-switch-lm2/1)# switchport false -------------------------------------------^ syntax error: unknown argument ruggedcom(config-switch-lm2/1)# |
Follow us on