(0)| 5/1/2023 12:24 PM | |
|
Posts: 7 Rating:
|
I am new to whole world of PLC programming and Industrial application. Recently I have using a TIA V17 PLC application for testing a vendors Profinet firmware. I noticed 2 different behaviour.. Scenario : A batch of 32 drives are connected in Daisy Chain network with I/O cycle set as 1 ms using 1500 PLC. When all drives came online – we disconnected any drive say 7thin sequence and observed that drives 1-6 at random showed flickering “Fieldbus Warning” warnings / connect – PLC connect / disconnect messages. Note that we have set Watchdog timer 3ms for all drives. We observed that when we remove the cables connection as in [New Topology Changes View.png] wrt old Topology [Old Topology View] in Topology view of PLC program having 1ms I/O connection and 3ms Watch Dog timer – the issue in concern does not occur. Why do we see such a difference in between two different topologies - do we need to correct some config in [Old Topology View]? Is it a PLC Application issue or issue with the Firmware? AttachmentNew Topology Changes View Vs Old Topology View.docx (512 Downloads) |
| 5/2/2023 4:38 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject TIA V17 PLC Application Topology View is published within the conference Communication / Networks. Jen_Moderator |
This contribution was helpful to
|
|
Follow us on