(0)| 5/9/2023 7:22 AM | |
|
Joined: 8/29/2019 Last visit: 9/12/2024 Posts: 7 Rating:
|
Dear Sir, Do you have a firmware V1.2 of OP77A? Thans alot.! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/09/2023 11:52:27New subject after splitting |
|
| 5/11/2023 1:24 PM | |
|
Joined: 8/3/2009 Last visit: 1/22/2026 Posts: 16654 Rating:
|
Hello The main question is which WInCC flexible or Protool Version do you use to program this Panel?? The IMage Version 1.2 was used with WinCC flexible 2005!!! Have a look here: https://support.industry.siemens.com/cs/de/de/view/21742389 So in WinCC Flexible you can only transfer a project if the specific image version is loaded to the panel if not then you have to do a image update. So if you load that panel with a newer Flexible version then a OS Update to that coresponing image version will be made. You cannot choose free the image version, its always bonded to the WinCC flexible Version. Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on