(0)| 5/17/2023 8:28 PM | |
|
Joined: 2/3/2022 Last visit: 1/15/2026 Posts: 14 Rating:
|
Hi all, I have an application where its used a Sinamics G120 and an S7 1511 to control a machine, we are using standard v/f control as it covers the application. To measure the actual speed of the material travelling on the machine we have a system with a encoder, wich rotates over the material as soon as a pneumatic system is enabled and press the encoder on the material. The encoder used is a Drive-CliQ encoder as we have a Sinamics G120 CU250S-2. So question is: Is it possible to adjust the telegram of the drive (adding supplementary words), and use that encoder in the CPU side as an external encoder. Following the principles in the FAQ: SINAMICS S120 and SIMATIC S7-1500(T): How to connect a 2nd encoder via Startdrive... - ID: 109793754 - Industry Support Siemens Thank you all in advance. |
Last edited by: Jen_Moderator at: 05/22/2023 08:32:00Link optimized. |
|
Follow us on